Configuring Analog Points

The Sofrel driver supports Sofrel Analog Input and Analog Output points. To configure the properties for each analog point use the fields on the Sofrel Analog Input Point Form, or the Sofrel Analog Output Point Form, as appropriate.

This section covers configuration of properties on the Analog Point tab of each Form, and the properties on the Control tab of the Sofrel Analog Output Point Form. For information on the fields on other tabs, see Tabs on Point Forms.

For Analog Input or Analog Output points, use the Analog Point tab to:

For Sofrel Input points

Use the Input tab to:

For Sofrel Analog Output points

Use the Control tab to:

Use the Control Checks tab to:

Related Topics Link IconFurther Information


Disclaimer

Geo SCADA Expert 2020