Configuration Mimic

The example project includes a Configuration Mimic.

The Mimic displays configuration information about the Totalflow. You can also do things like changing the gas composition or orifice plate diameter for each run. When you change the gas composition for a run, you will need to click the Refresh button to see the updated values.

Click on a value to display the context-sensitive menu for the underlying point. You can use the menu options to locate the point in the database, reconfigure the point by opening its Properties window, and so on.


Disclaimer

Geo SCADA Expert 2020