CurrentData Mimic

The example project includes a CurrentData Mimic.

The Mimic shows current data from the Totalflow. Click on a value to display the object menu for the underlying point. You can use the menu options to locate the point in the database or open its Properties window to see how it is configured.


Disclaimer

Geo SCADA Expert 2020