DeviceConfiguration Group

The example project includes a DeviceConfiguration group.

This group contains points that are configured to show different types of information about a Totalflow. The intent of this group is to demonstrate how to use the Geo SCADA Expert Totalflow Driver to read configuration information from a Totalflow device.

Some points, like ContractHour, have the Control aggregate enabled. You can right-click on this point, select the Control option, and enter a new contract hour for the Totalflow device.

The points in this group are displayed and manipulated from the Configuration Mimic in the Mimics group. Each of the points in this group are attached the ScannerConfig scanner.

Further Information

Digital Point Control Tab

Numeric Point Control Tab

String Point Control Tab


Disclaimer

Geo SCADA Expert 2020