Delete a Y-Axis
Each Trend can display multiple Y-Axes as required. If you need to remove a Y-Axis from a Trend:
- Display the Trend that has the Y-Axis that you want to remove (see Display a Trend in Design Mode).
- Right-click on the Y-Axis that you want to remove.
A context sensitive menu is displayed. - Select Delete.
The selected Y-Axis is removed from the Trend display. - Save the configuration.
Any traces that use the deleted Y-Axis are also removed from the Trend when you delete that Y-Axis. For this reason, you should assign traces to a Y-Axis that will remain on the Trend (see Configure a Trace).