Hide and Show the Axes

You can choose to hide any of the axes so that the Trend makes more use of the display area.

To hide and show the axes:

  1. Right-click in the main display area on the Trend.
    A context sensitive menu is displayed.
  2. Disable the Show X Axis option.
    The X-Axis is removed from the Trend.

    Trend showing no X-Axis

  3. Right-click in the main display area on the Trend.
    A context sensitive menu is displayed.
  4. Enable the Show X Axis option.
    The Trend redisplays the X-Axis.
  5. Right-click in the main display area on the Trend.
    A context sensitive menu is displayed.
  6. Disable the Show Y Axis option.
    If you have multiple Y-Axes on your Trend, a further context sensitive menu is displayed.

    You can enable or disable individual Y-Axes, enable All to display all Y-Axes, or enable None to display no Y-Axes.

  7. Enable the None option.
    Thee Trend’s axes are hidden.

    Trend showing no axes

  8. Right-click in the main display area on the Trend.
    A context sensitive menu is displayed.
  9. Disable the Show Y Axis option.
    If you have multiple Y-Axes on your Trend, a further context sensitive menu is displayed.
  10. Enable the All option.
    The Trend displays all of the Y-Axes.

Disclaimer

Geo SCADA Expert 2020