Zoom Out on a Trend

To zoom out on a Trend’s trace(s) or X-Axis either:

  1. Display a Trend in Run Mode.
  2. Either:
    • Select the Zoom Out command from the Navigation group on the ribbon's Home tab.
      The Trend is magnified so that the X-Axis shows a longer time range.

    Or:

    • Press the F8 function key.
      The Trend is magnified so that the X-Axis shows a longer time range.

    Or:

    • Position the cursor over the X-Axis or main display area of the Trend then roll the mouse wheel backwards (this is only available if your mouse has a wheel).
      The Trend is magnified so that the X-Axis shows a longer time range.

    Or:

    • Right-click on the X-Axis or main display area of the Trend to display a context sensitive menu, then select the Zoom Out option from the context-sensitive menu.
      The Trend is magnified so that the X-Axis shows a longer time range.

To zoom out on a Y-Axis:

  1. Display a Trend in Run Mode.
  2. Either:
    • Right-click on the Y-Axis to display a context sensitive menu, then select the Zoom Out option from the context-sensitive menu.
      The Y-Axis is magnified so that it shows a wider range of values.

    Or:

    • Position the cursor over the Y-Axis, then roll the mouse wheel backwards (this is only available if your mouse has a wheel).
      The Y-Axis is magnified so that it shows a wider range of values.

Disclaimer

Geo SCADA Expert 2020