Add a Folder to your Favorites List

Ideally, you should organize the links in your Favorites List, so that they are grouped in folders. This improves the efficiency of the Favorites feature, as it allows you to structure your links into logical groups, rather than have the entries appear in a long list.

To add a folder to your Favorites List, either:

  1. Right-click on an entry in your Favorites List. (To add a folder to another folder, right-click on the existing folder.)
    A context sensitive menu is displayed.
  2. Select the New Folder option.
    A new folder is added to your Favorites List. The folder is selected automatically, ready for you to define its name.

Or:


Disclaimer

Geo SCADA Expert 2020