Zoom Out on an X-Y Plot

To reduce the level of magnification on an X-Y Plot so that more data is shown (but in less detail):

  1. Display an X-Y Plot in Run Mode.

    The Zoom Out tool is also available when you are configuring the X-Y Plot in Design mode.

  2. Either:
    1. Right-click above the X-Axis or to the right of the Y-Axis to display a context-sensitive menu.
    2. Select the Zoom Out option.
    3. Repeat as necessary.

    Or:

    1. Select the Home tab on the ViewX ribbon.
    2. Select the Zoom Out command from the relevant command group.
    3. Repeat as necessary.

    Or:

    1. Press the F8 function key.
    2. Repeat as necessary.

    Or:

    • Roll the mouse wheel backwards until the required level of magnification is shown.

Zooming out on the X-Y Plot will reduce the level of magnification on the X-Y Plot so that you can see more data but in less detail.

To increase the level of magnification, you need to use the Zoom In tool (see Zoom In on an X-Y Plot).


Disclaimer

Geo SCADA Expert 2020