Change the Position of the Axes

You can change the positions of the axes on an X-Y-Z Plot. To do this:

  1. Right-click on the relevant axis.
    A context-sensitive menu is displayed.
  2. Select the Show Axes option.
    A further context-sensitive menu is displayed.
  3. Select the required axis position(s) from the options offered. The options vary, depending on the type of axis, but include a combination of the following (you can select more than one):
    • Back Axis:The axis is positioned to the back of the Time axis.
    • Front Axis:The axis is positioned to the front of the Time axis.
    • Left Axis:The axis is positioned to the left of the x-axis.
    • Right Axis:The axis is positioned to the right of the x-axis.

Example:

An X-Y-Z Plot with the Time axis displayed to the left and the x- and y-axes displayed to the front:

The same X-Y-Z Plot with the axes displayed in both positions (the x- and y-axis to both the Front and Back, and the Time axis to both the Left and Right):

The same X-Y-Z Plot with the x-axis displayed in both positions, the y-axis at the back, and the Time axis to the right:

Further Information

If you are working with an X-Y-Z Plot in Design mode, you can also adjust the length and angle of the Time axis (see Adjust the Time Axis).


Disclaimer

Geo SCADA Expert 2020