Define an Outstation’s Shared Properties

The Outstation Form for Shared outstations includes a Shared tab.

Shared outstations communicate with the Geo SCADA Expert server using one of two direct channels (see Shared Outstations). The channels are referred to as Line A and Line B. You define which channels you want to use as Line A and Line B, using fields on the Outstation Set tab of the relevant Outstation Set Form (see Defining Channel Settings for a Shared Set).

For information on the use of the fields on the Shared tab of the Shared Outstation Form, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.

For any Shared outstation fields not described in the above sections, see the driver-specific documentation.


Disclaimer

Geo SCADA Expert 2020