Defining any Default Pre- and Post-Amble Message Settings for a Channel

Some communications equipment or media require ‘padding’ or specific digits (an additional message) to be inserted at the start and/or at the end of each message that is transmitted using that equipment or media. Prefixed digits or padding are referred to as Pre-Amble and suffixed digits or padding as Post-Amble. Pre- and Post-Ambles comprise an even number of digits, so giving a whole number of bytes. Pre- and Post-Ambles are typically used to help to prevent messages from being ‘clipped’ (truncated). However, some communications equipment may use Pre- and Post-Ambles to correctly interpret both the start and end of each transmitted message (or ‘data packet’), or to specify a delay to allow a channel to synchronize before any data is transmitted.

If Pre- and Post-Ambles are required, the actual digits that you need to specify differ, depending on:

If an advanced driver supports Pre- and Post-Ambles, the Channel Form(s) for the driver include an additional Pre/Post Amble section on the Scan Parameters tab. Use the fields within the Pre/Post Amble section to specify the Pre- and Post-Ambles that need including for any transmissions via that channel.

Should a particular outstation use different Pre- and/or Post-Amble bytes to those specified on the channel (for instance, if a radio communicates with that outstation at a different frequency to the other outstations on the channel), you can override the channel’s default Pre- and Post-Amble settings with outstation-specific settings for that particular outstation (see Define any Pre- and Post-Ambles for an Individual Outstation).

The Pre- and Post-Ambles configured in Geo SCADA Expert are only applied to messages that Geo SCADA Expert’s drivers transmit, rather than receive, via a channel.

ATTENTION: Pre-ambles on messages received via network-connected channels are only supported when Geo SCADA Expert initiates the connection.

The Pre/Post Amble section on the Channel Form contains these fields:


Pre-amble

Use to specify any bytes that are required at the start of each message that the driver transmits via this channel.

Leave the field empty if no pre-amble is required.

Post-amble

Use to specify any bytes that are required at the end of each message that the driver transmits via this channel.

Leave the field empty if no post-amble is required.

Where a Pre- and/or Post-Amble is required, specify that pre- or post-amble as a sequence of hexadecimal digits. Each pair of digits forms a byte in the pre- or post-amble. Ensure that the number and type of digits specified are suitable for both the protocol and type of communications media being used. (Hexadecimal format is base 16 and can include the digits 0, 1, 2, 3, 4, 5, 6, 7, 8, 9, A, B, C, D, E, and F. Each digit is a nibble (half a byte), therefore you should always specify pairs of digits.)

Refer to the documentation supplied with your communications equipment for the number of bytes (pairs of digits) that you need to specify. The padding will probably be specified as a time—to ascertain the number of bytes that you need to specify to allow for the required padding time, you will need to Calculate the Time that a Channel Takes to Transmit each Byte of Data.

Refer to the driver- or product-specific documentation for information on any protocol-specific limitations or requirements.

ATTENTION: Some protocols require each message to begin with a particular sequence of bytes. Do not use such bytes as Pre- or Post-Amble padding. Refer to the driver- or product-specific documentation for further details.


Disclaimer

Geo SCADA Expert 2020