<Dynacard Type> Dynacard
Associated with: Dynacard Stores
The name of this status attribute indicates the type of dynacard for which a set of data is stored online (for example, ‘Last Stroke Dynacard’). The status attribute displays the date and time at which Geo SCADA Expert uploaded the set of dynacard data to the Dynacard Store.
For those types of dynacard for which the Dynacard Store can only retain one set of data online, the status attribute displays the value Not Present if Geo SCADA Expert has never uploaded that type of dynacard data to the Dynacard Store.
3 Stored Dynacard: 21/Jun/2012 16:09:56.031
(The ‘3’ indicates that this status attribute relates to the third set of ‘Stored’-type dynacard data associated with this particular Dynacard Store. Geo SCADA Expert uploaded the set of data at 16:09:56.031 on 21st June 2012.)
Use the status attribute in conjunction with the relevant Number of Points and Outstation Timestamp status attributes.