Monitoring the State of Direct Communications on your System
            You can use Status displays to check on the status of individual channels or outstations (see Status Displays), and 
- Channel Scanning Statistics List
 - Channel Serial Port Statistics List
 - Outstation Comms. Statistics List.
 
The Lists are available from the Queries Bar.