Configuring String Points
The Geo SCADA Expert Advanced Modbus driver supports String points.
On the Advanced Modbus driver, you use String points to retrieve data for which the value is a text string.
Configure the properties of each string point using the fields on the Advanced Modbus String Point Form.
This section covers configuration of properties on the String tab of the Advanced Modbus String Point Form. The properties on other tabs are common to points on many advanced drivers (see Tabs on Point Forms).
Use the String tab to: