Specify the Port Number to Communicate with a Remote Application

Use the Port field on the Connection tab to specify the TCP/IP port number that Geo SCADA Expert uses to listen for commands from the application software.

The default is 49155. Specify the required number, typically in the range 1025 to 65535 (numbers 1 to 1024 are reserved for special use).

Where only one Remote Connection exists on a system, you can leave this setting at its default. Where multiple Remote Connections exist, specify a different Port number for each connection.


Disclaimer

Geo SCADA Expert 2020