Configuring an Advanced Trio Diagnostics Radio Channel
You use an Advanced Trio Diagnostics Radio Channel in the database to represent a communication connection between the Geo SCADA Expert server and a Trio radio (or hot-standby controller unit, in the case of a hot-standby radio setup).
To create and configure a Channel database item, you need to be logged on to Geo SCADA Expert with a User account that has the Configure Database feature enabled and the relevant permissions set (see Creating a User Account in the Geo SCADA Expert Guide to Security).
The number of channels that you need to configure, along with the channel's Connection Type and setup varies, depending on the radio Series, the chosen interface, and Geo SCADA Expert's access to the radios in the radio network (see Required Communication Setups).
You configure the Channel database item by using the Advanced Trio Diagnostics Radio Channel configuration Form (see Display a Form in the Geo SCADA Expert Guide to Core Configuration). The Form includes a number of tabs. The tabs and the properties on those tabs are common to channels on many drivers (see Tabs on Channel Forms in the Geo SCADA Expert Guide to Advanced Drivers).
Further Information
Configuring a Channel in the Geo SCADA Expert Guide to Advanced Drivers. (A Trio Radio Channel is a Direct channel.)