Clear the Value of an Argument

To clear the value that is specified for an argument in the Edit Method window, the Add Action window, or the Edit Action window, either:

  1. Right-click on the argument in the Arguments list.
    A context-sensitive menu is displayed.
  2. Select the Clear option.
    The Value is cleared.


Or:

  1. Double-click on the argument in the Arguments list.
    The Expression window is displayed.
  2. Delete the expression from the Expression window.
  3. Select the OK button on the Expression window to confirm the deletion.
    The Expression window is closed and the argument’s value is cleared.

Disclaimer

Geo SCADA Expert 2020