Configure the Properties on the Time Profile Form

To configure the Time Profile’s properties, you need to display the Time Profile Form (see Display a Form).

The Time Profile Form has several tabs.

Use the Identification tab to configure the Time Profile’s Identification properties (see Defining Identification Details).

Use the Location tab to specify the item's geographical coordinates. (You need only configure the properties on this tab if your system uses Geo SCADA Expert's Geographical Location features.)

Use the User Methods tab to define any custom pick actions (‘methods’) for the Profile (see Using the User Methods Tab to Define Custom Actions).

Use the Profile tab to configure the Profile-specific properties. For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.


Disclaimer

Geo SCADA Expert 2020