Define the Trend Properties

You can display the trend, or movement, of a Forecast’s values in the form of a Trend. (A Trend is a type of graph used to compare values over time).

Each Trend consists of an x-axis, a y-axis, and a trace. The x-axis displays a time interval, and the y-axis displays the measurement units. The Trace represents the Forecast values.


Once Forecast data has been imported into a Forecast object, you can view the data as a Trend by using the Display <Trace Name> Trend pick action, available from the Forecast object. (The pick action only becomes available once data exists for a Forecast object.)

Use the fields within the Trend section of the Forecast tab to define the settings for when the data is displayed as a Trend:


Disclaimer

Geo SCADA Expert 2020