Display the Calendar Editor

You use the Calendar Editor to select the Calendar year and allocate holidays or other special day types, as needed.

To display the Calendar Editor:

  1. Display the Database Bar (see Display an Explorer Bar).
  2. Double-click on the item in the Database Bar (if you are logged on as a user that has the Double Click Edits Documents feature enabled).
    The Calendar Editor is displayed.

Alternatively, you can display a Calendar in Design mode by performing one of the following:

  1. Right-click on the Calendar entry in the Database Bar.
  2. Select the Edit Calendar option.

or:

  1. Right-click on the Calendar entry in a Queries List.
  2. Select the Edit option.

or:

  1. Select an animated representation of the Calendar on a Mimic. (Provided that the animated representation is associated with the Calendar’s Pick Action Menu and provides access to the relevant menu option).
  2. Select the Edit option.

You can use the Calendar Editor to:


Disclaimer

Geo SCADA Expert 2020