Trend - Validated/Good Data

Associated with: Trends and X-Y-Z Plots

The Validated/Good Data state is indicated by a light green marker (by default) on a Trend or X-Y-Z Plot’s trace.

The color indicates that the value is reliably accurate.

With Trends on systems on which manual Historic Validation is enabled, the color indicates that the value has been validated by an operator or engineer. (With Trends on systems on which manual Historic Validation is not enabled, the color indicates that the value is reliably accurate.)

For data sources that exist in the Geo SCADA Expert database, Geo SCADA Expert obtains the marker color from the data source's Color Palette. The exception to this is if Geo SCADA Expert is unable to obtain the marker color from the server (for example, if communications with the server is interrupted when a Trend is redrawn). In such a situation, Geo SCADA Expert uses the marker color that is specified in the Options window. Geo SCADA Expert also uses the marker color from the Options window for data sources that are from a non-Geo SCADA Expert database (for example, another OPC database).

Further Information

Validating historic data:

X-Y-Z Plots: see the Geo SCADA Expert Guide to X-Y-Z Plots.


Disclaimer

Geo SCADA Expert 2020