Calculation Points

Calculation Points are a special type of internal point that you can use to perform simple calculations on data in the Geo SCADA Expert database. Geo SCADA Expert derives a value for a Calculation Point by evaluating an expression. An expression is a combination of references to database items (tags), symbols and operators. The expression can include conditions as well as arithmetic and logical functions.

Internal points together with Logic functions can be used to perform calculations in a similar way to Calculation points, but are used for more complex calculations.

Geo SCADA Expert supports four types of Calculation Point:

You can specify when Calculation points should evaluate expressions:

Further Information

Configuring and Working with Calculation Points

Expressions: see Welcome to the Guide to Expressions in the Geo SCADA Expert Guide to Expressions.

Internal Points:see Internal Points

Tags: see Tags in the Geo SCADA Expert Guide to Expressions.

Configuration point pick actions: see Using Calculation Point Specific Actions.


Disclaimer

Geo SCADA Expert 2020