Configuring Analog Points

The DDE driver supports Analog Input and Analog Output points.

The points are used to map ‘point’ data on DDE servers into Geo SCADA Expert in a format that it can understand, and vice versa.

Configure the properties of each analog point using the fields on the DDE Analog Point Form.

This section covers configuration of analog-specific properties on the DDE tab of the Form.

Use the fields on the DDE tab to:

For information on the fields on the Analog Point tab, see Defining Analog Point Details in the Geo SCADA Expert Guide to Core Point Configuration.

If the point is an output point, you also need to enable and configure the properties on the Control tab—for information, see Define the Control Settings for an Analog Output Point in the Geo SCADA Expert Guide to Core Point Configuration. You can also optionally use the Control Checks tab to configure the Control Checks settings (see Configuring Control Checks Settings in the Geo SCADA Expert Guide to Core Point Configuration).

For information on the fields on other tabs, see Tabs on Point Forms in the Geo SCADA Expert Guide to Simple Drivers.


Disclaimer

Geo SCADA Expert 2020