Configuring Time Points

Use DDE Time points to map time values on DDE servers into Geo SCADA Expert.

Configure the properties of each Time point using the fields on the DDE Time Point Form.

For information on the Time Point tab on the Time Point Form, see Defining Time Point Details in the Geo SCADA Expert Guide to Core Point Configuration.

For information on the fields on the DDE tab, see Configure Common Properties on the DDE Tab.

For information on the Control tab on the Form, see Define the Control Settings for a Time Point in the Geo SCADA Expert Guide to Core Point Configuration.

For information on the fields on other tabs, see Tabs on Point Forms in the Geo SCADA Expert Guide to Simple Drivers.


Disclaimer

Geo SCADA Expert 2020