Specify NetDDE Properties

The DDE server with which Geo SCADA Expert communicates can reside on the same or another node to the server(s) on which the Geo SCADA Expert database resides.

Use the fields within the NetDDE section of the DDE tab to specify whether the DDE server is on the same node as the Geo SCADA Expert database, or is a NetDDE server that is to be accessed remotely via a network.

Where Geo SCADA Expert is to access a remote NetDDE server, you need to specify the user name, password, and domain of a user that has a valid logon to both machines (the Geo SCADA Expert server and the DDE server).


Disclaimer

Geo SCADA Expert 2020