Which Driver?

Geo SCADA Expert is able to communicate with Allen-Bradley controllers using one of several Geo SCADA Expert drivers. Which driver you use depends on your system set-up, configuration requirements, and the type(s) of Allen-Bradley controllers with which Geo SCADA Expert is to communicate.

The EtherNet/IP driver enables Geo SCADA Expert to use the EtherNet/IP protocol to communicate with certain ranges of Allen-Bradley controllers.

The DF1 driver enables Geo SCADA Expert to use the DF1 protocol to communicate with Allen-Bradley controllers.

With new installations in which the Allen-Bradley controllers are supported by both drivers, we recommend that you use the EtherNet/IP driver. This latter driver will give you more flexibility should your system requirements change in the future.

With Allen-Bradley controllers that are from ranges that are not supported by the EtherNet/IP driver, or with which you want Geo SCADA Expert to communicate using the DF1 protocol, use the DF1 driver.

For information about the other Geo SCADA Expert drivers that can be used to communicate with Allen-Bradley controllers, please contact your Schneider Electric agent.

Further Information

Supported Drivers and Protocols.


Disclaimer

Geo SCADA Expert 2020