DNP3

Binary Point States

Use the fields within the States section of the Binary Point tab to define state-related information for the point, such as the handling of state-related alarms.

The Number of Bits, defined toward the top of the Binary Point tab, determines the number of state fields that are available for use.

For information on configuring binary point states, see Define the Point States for a Digital Point.


Disclaimer

Geo SCADA Expert 2020