Class n Poll Statistics
            Associated with: DNP3 master outstations
The Class 1 Poll Statistics, Class 1 Poll Statistics, and Class 2 Poll Statistics attributes show the number of attempted and successful DNP3 Class Event Polls issued by the Geo SCADA Expert DNP3 driver to the outstation, since the statistics were last reset.
You can reset the statistics using the Reset Poll Statistics pick action. If the poll statistics have been reset, two sets of Poll Statistics attributes are displayed for each class. The first displays the statistics since the last reset of poll statistics; the second displays the statistics between the previous two resets.
Example:
5 attempted, 5 successful since 04/Nov/2003 11:36:49.255
If the statistics have been reset, a second entry will display statistics in the form:
25 attempted, 23 successful between 14/Oct/2003 11:35:32.261 and 04/Nov/2003 11:36:49.255