DNP3

Define the Filtered Value Map Locations

DNP3 slave outstations use Filtered Value Maps to store ‘point’ data. The source of the Value Map data typically comes from another source, such as a Modbus device or an OPC source, and is mapped into Geo SCADA Expert in order to enable the DNP3 master to extract the required data from that device, using the DNP3 protocol.

You need to specify the Filtered Value Maps that each Slave outstation uses, and the location of those Filtered Value Maps within the Geo SCADA Expert database. The Filtered Value Maps that you use for the Slave outstation have to exist on your system and be suitably configured (see Configuring Value Maps in the Geo SCADA Expert Guide to Core Configuration).

Use the fields within the Value Maps section of the DNP3 tab to define the Filtered Value Maps that are associated with the DNP3 slave outstation.

Leave the fields blank for any Map types that are not used by the Slave outstation.

Use the fields within the Static Objects section of the tab to Specify the DNP3 Static Object Types that the outstation uses to send current data to the DNP3 master. Use the fields within the Event Objects section of the tab to Specify the DNP3 Event Object Types that the outstation uses to report event data to the DNP3 master.


Disclaimer

Geo SCADA Expert 2020