Device Trouble Alarm
            Associated with: DNP3 master outstations
The Device Trouble Alarm attribute indicates whether the outstation’s DNP3 DEVICE_TROUBLE IIN bit is set. This bit is typically set when there is a hardware problem at the outstation.
Possible states: Displays one of the Standard Alarm States.
See the outstation documentation for information on clearing the Device Trouble IIN bit.