Freeze and Clear
            Associated with: DNP3 master outstations that support Frozen Counter points
Security permission required to access this pick action: Diagnostics
Use the outstation’s Freeze and Clear pick action to copy the values of the Counter Points to their associated Frozen Counter Points, and then reset the Counters back to a pre-configured value. The reset value is determined by the Slave and is typically zero.
The pick action takes into account the Freeze settings configured on the Outstation Form (see Configure Frozen Counter Support).
Also see Freeze.
If using this pick action with the Automation Interface, you need to specify the method name FreezeClear.