Read Device Attributes
Associated with: DNP3 master outstations
Security permission required to access this pick action: Retrieve Data
Use the Read Device Attributes pick action to request Geo SCADA Expert to read an outstation’s Device attributes and store the results in the Geo SCADA Expert database.
In addition to this pick action, the Read Device Attributes field on the DNP3 Outstation Form can be used to specify whether Geo SCADA Expert is to read an outstation’s Device attributes automatically, whenever communications are established with that outstation (see Configure the Actions that Occur on Communications Startup).
You can view the uploaded attributes using the Outstation’s Status display window (see DNP3 Outstation Status Attributes). The attributes are also available as OPC properties (see the Database Schema and the Geo SCADA Expert Guide to the Database).