DNP3

Which Driver?

Some DNP3 devices support additional features that are unavailable on other DNP3 devices. To support these additional features, Geo SCADA Expert uses a DNP3 extension driver. If your system uses a DNP3 extension driver, use the guide to that extension driver in conjunction with this guide. In each case, your system needs to run the DNP3 driver, along with the relevant extension driver.

The DNP3 extension drivers that Geo SCADA Expert supports include:

To use the DNP3 protocol to communicate with devices other than those mentioned above, you use the DNP3 driver on its own.

Further Information

Supported Drivers and Protocols.


Disclaimer

Geo SCADA Expert 2020