BOOTP Table Arguments
            Use these arguments for updating a row in a BOOTP table (for further information, see Add and Configure the Entries in a BOOTP Table):
- Row (Byte)—Specify the row number within the table (1 to n).
 - HardwareAddr1 to HardwareAddr6 (Byte)—Use these six arguments to specify the separate parts of the hardware address of the Ethernet device for which the SCADAPack E outstation is to remotely configure an IP address.
				
Example:
To specify the hardware address 00:1A:2B:3C:4D:5E, enter:
HardwareAddr1 as 00
HardwareAddr2 as 1A
HardwareAddr3 as 2B
and so on. - IPAddress (Long)—Specify the required IP address for the Ethernet device.
                
Example:
For the IP address 192.168.1.97
Convert each octet into its hexadecimal equivalent
192 (dec) = C0 (hex)
168 (dec) = A8 (hex)
1 (dec) = 01 (hex)
97 (dec) = 61 (hex)Create the hexadecimal long equivalent
C0A80161Convert to decimal (using ‘Calculator’ for example)
3232235873