Configure Ethernet DNP/IP Properties
            Use the fields in the Ethernet DNP/IP section of the SCADAPack TCP/IP tab to specify the DNP3 Data Link configuration for frames transmitted through either of the SCADAPack E outstation’s ethernet ports.
                
            
For information on configuring these properties, see Configure Data Link Layer Properties.