Configure General Properties
            Use the fields at the top of the Binary Point tab to define the general properties of a DNP3 SCADAPack binary point. For further information on most of these properties, see Configure Common Properties of DNP3 SCADAPack Points in this guide, and see Configure General Properties in the Geo SCADA Expert Guide to the DNP3 Driver. Properties that are specific to DNP3 SCADAPack Binary points are explained below:
                
            
- RTU Event—Applies only if the point’s Point Data Class is set to Class 1 Event, Class 2 Event or Class 3 Event (see Configure Common Properties of DNP3 SCADAPack Points).
        
        
Use the RTU Event combo box to specify whether the outstation just stores the event, or immediately generates an unsolicited message whenever the point changes state (see Specify Whether a Class n Event Triggers an Unsolicited Message).