Configure any Physical Binary Input Point Properties
            Use the fields located at the top of the Input tab on the DNP3 SCADAPack Binary Input Point Form to specify how the SCADAPack E outstation processes the binary point when it has a Point Type of Physical Input (see Configure Common Properties of DNP3 SCADAPack Points).
                
            
- Invert Point State—If you select this check box, the outstation inverts the raw state of the physical input. The inversion is performed before any other processing such as Persistence into/out of Alarm.
 - De-bounce Time—Use to specify the time that a raw physical input has to remain in the same state before the outstation considers the point as being in that state.
            
You typically set the De-bounce Time to a few milliseconds and use it to filter out ‘chatter’ from physical switches.
Enter the time in the OPC Time Format.