DCD Drop Outs

Associated with: DNP3 SCADAPack Status Information items that are configured to retrieve Port Status information.

This status attribute indicates the number of Data Carrier Detect (DCD) drop outs that have occurred on the port.

The attribute only applies if the port’s Function is set to PPP/TCPIP. (The status attribute’s value remains at zero for any ports that are assigned a different Function.)


Disclaimer

Geo SCADA Expert 2020