Downloaded Firmware Image
            Associated with: DNP3 SCADAPack E Outstations and DNP3 SCADAPack Remote E Outstations.
The status attribute indicates:
- The name of the last .biz file to be downloaded to the outstation.
 - A time stamp showing the last modification date and time of the SCADAPack E .biz file from which the downloaded Firmware Image file was obtained.
 
The attribute is only displayed if the Download Firmware, or Download Remote Firmware pick actions have been used to successfully download an operating system firmware file to the outstation. (Each firmware file comprises a SCADAPack E .biz file that has been imported into Geo SCADA Expert using a DNP3 Firmware Image database item.)
For more information, see Using Geo SCADA Expert to Import and Download SCADAPack Outstation Firmware Image Files.
Example:
"761e586.biz" Modified at 22/10/2008 10:38:58.000
(Indicating that the last Firmware Image file to be downloaded to the outstation was the file named ‘761e586.biz’. The SCADAPack E .biz file from which the Firmware Image file was obtained was last modified on the date and time indicated above.)