Input Power Low
Associated with: DNP3 SCADAPack Status Information items that are configured to retrieve SCADAPack ES Remote I/O information.
This status attribute indicates whether the power being used to run the remote I/O module is low.
Possible states: True, or False.
Do not confuse this status attribute with the Internal Battery Low attribute.