Link Confirm Timeouts
Associated with: DNP3 SCADAPack Status Information items that are configured to retrieve Port Status information.
The status attribute indicates the number of times that a confirmation was expected, but was not received, for DNP3 data link frames that have been transmitted using this port.
This status attribute only applies if the port’s Function is set to DNP3.