Map to Point Data on a SCADAPack ES Remote I/O Module
            When Mapping to point data on a SCADAPack ES Remote I/O module, use these fields to specify the physical location of the point on that module:
                
            
- I/O Source—Use to Specify the I/O Module, I/O Card, or Remote Outstation on Which the Point is Located.
 - Remote Point Number—Use to Specify the Location of the Point on the I/O Module, I/O Card, or Remote Outstation.