Profile ID
            Associated with: DNP3 SCADAPack points and pulse actions with which Profiles are associated.
This status attribute indicates the combination of Profiles used by a point or pulse action on a particular outstation. Each DNP3 SCADAPack Outstation can support up to 999 unique combinations of Profiles. Geo SCADA Expert allocates each point’s and pulse action’s Profile ID automatically, based on the combination of Profiles used by that particular point or pulse action and, for DNP3 SCADAPack Counter Points, the point’s Multiplier.
The attribute is only displayed if a pulse’s action(s), or any of a point’s limits and/or current value are profile-controlled (see Specify Whether any Profiles are Used to Change a Point’s Limits or Current Value). The status attribute is displayed regardless of Profile Type.
Example:
5