RemoveFile
            Associated with: DNP3 SCADAPack E outstations and DNP3 SCADAPack Remote E outstations.
Security permission required to access this method: Configure.
UNEXPECTED BEHAVIOR OF APPLICATION
Use the RemoveFile method with care. Ensure that the file is no longer required or in use before attempting to remove the file from the database.
Use this method to remove a file from a DNP3 SCADAPack E outstation in the Geo SCADA Expert database.
This method is the equivalent of removing a file by using the Remove button on the Configuration Setup window (see Remove a File from a SCADAPack E Outstation’s Configuration).
Argument:
- FileName (String)—Specify the name of the file that is to be removed from the Geo SCADA Expert database.