Specify how the SCADAPack Outstation Handles Underrange, Overrange and Invalid RTU Events
            The Out of Range RTU Event field is displayed at the bottom of the Alarm Limits section on the Analog Point tab:
                
            
- Out of Range RTU Event—Applies only if a point’s Point Data Class is set to Class 1 Event, Class 2 Event or Class 3 Event (see Configure Common Properties of DNP3 SCADAPack Points).
        
        
Use the Out of Range RTU Event combo box to specify whether the SCADAPack E outstation just stores the event, or immediately generates an unsolicited message whenever the point’s value becomes Underrange, Overrange, or Invalid(see Specify Whether a Class n Event Triggers an Unsolicited Message).
 
If the Area of Interest feature is enabled on your system, an Area of Interest field is displayed below the Out of Range RTU Event field. For information on this property, see Specify the Area of Interest Associated with a Point’s State-Related Alarms and Events.