Specify the Outstation from which Geo SCADA Expert is to Retrieve Status Information
Use the Outstation field on the Parent tab to specify the DNP3 SCADAPack E outstation from which Geo SCADA Expert is to retrieve status information:
Use the field’s browse button to display a Reference browse window. Select the required outstation entry from the window.