Specify the SCADAPack Properties
            Use the fields on the SCADAPack tab of each DNP3 SCADAPack E Outstation Form to:
- Configure Automatic Configuration Download
 - Specify Whether to Ignore an FC Not Implemented Error
 - Specify Whether a Download Configuration Request Requires Confirmation
 - Specify the IEC 61131-3 Version Running in the Outstation
 - Specify the Outstation Identification Strings
 - Configure the Unsolicited Message Properties that are Specific to a Particular DNP3 Master
 - Configure Unsolicited Message Generation
 - Configure Event Configuration
 - Configure the DNP Route Table and Modem Authentication Properties
 - Configure the Data Link Layer Setup Properties
 - Configure Application Layer Properties
 - Configure Network Access Parameters
 - Configure the Modem Parameters
 - Configure the Trend Retrieval Properties
 - Configure Data Concentrator Properties
 - Configure Modbus Properties
 - Configure SCADAPack ES Remote I/O Properties
 - Configure the Profiler and ISaGRAF Time Zone Properties
 - Specify the Profile Type
 - Configure Low Voltage Alarm Level
 - Configure the Control/Status Properties
 - Configure Scratchpad String Points
 - Configure the Firmware Image Properties
 - Configure the Security Configuration Properties.