TCP/IP Routing
            You can configure a SCADAPack E outstation to route TCP/IP packets between multiple networks.
The outstation is capable of routing between Ethernet and Serial (PPP) on multiple interfaces.
                
            
Further Information
Use an IP Route Table to Route TCP/IP Packets to Another TCP/IP Host.