Trip and Close Pulse Action Properties
            Use the fields within the Action section of the Trip/Close tab to define the configuration of the Trip and Close pulse actions.
                
            
The DNP3 SCADAPack Pulse Action (Trip-Close) point is effectively two independent SCADAPack Pulse Action (Trip-Close) points that are controlled by a single Geo SCADA Expert database point. For example, if you set the Pulse Count (see Configure Pulse Properties) greater than 1, you can send a control to the Close action while the Trip action is still executing. As with the DNP3 Pulse Action (Trip-Close) point, you cannot issue a Trip, for example, while the previous Trip action is still executing.
For further information, see Configure Trip and Close Pulse Actions in the Geo SCADA Expert Guide to the DNP3 Driver.